AnsweredAssumed Answered

Load AD9959

Question asked by Serg01 on Aug 1, 2018
Latest reply on Aug 1, 2018 by Serg01

Good Morning!

 

I try to load the registers of AD9959, but no signal on the output.

The sequence is shown on the figures:

 

At first the RST during 100 us, then trying to write 11 bytes in the AD9959. Load02.pg

 

For the beginning two bytes: 0x00 0x80, and IO_UPDATE pulse. Load02_1.jpg

 

Then 4 bytes 0x01 0xD0 0x00 0x00, and IO_UPDATE pulse. Load02_2.jpg

 

At the end, 5 bytes 0x04 0x33 0x33 0x33 0x33, and IO_UPDATE pulse. Load02_3.jpg (Frequency = 100 MHz)

But there are no signal on the Output of AD9959. What is wrong? How can I load the registers of AD9959?

Thank you very much.

Serg

Attachments

Outcomes