AnsweredAssumed Answered

Blackfin Image Processing Toolbox Performance

Question asked by Findl on Jan 10, 2012
Latest reply on Jan 11, 2012 by Findl

Hello,

 

I have got a question related to the performance of the Image Processing Toolbox presented within its documentation in comparison with the demo applications provided.

 

For Example the edge detection: The function "adi_sobel_3x3_horz_i8" is documented within the document "Image_Tool_Box_ProductSpecs_Rel1.4.0" on page 9 with a performance of 2.73cycl/pel (Memory Scheme 1) and 9.79 cycl/pel (Memory Scheme 2).

 

When I run the demo application "sobel_bf561" supplied with the Toolbox I can read the following performance measurements:

 

 

*******************************************************************
Input File: demo_512x512_yuv400.yuv
process => sobel 3x3 horizontal filter
Cycles/pel + DMA cycles = 127.839325
Only Func Cycles/pel = 119.797713
Output File: demo_512x512_yuv400_sobel_3x3_8_horz_output.yuv
*******************************************************************

 

If I compare the data provided within the documentation with the measurement data of the demo application, I recognize salient differences.

 

Can anybody explain that, please?

 

Regards Michel

Outcomes