AnsweredAssumed Answered

Need a LDO or DC-DC chip

Question asked by tolife on Jul 30, 2018
Latest reply on Aug 7, 2018 by Errgy

Now i am using AD7190 for designing my hardware. It is recommended to use ADP3303 in the reference doc of AD7190 . But the ADP3303 do not meet my requirements.

 

My requirements as below:

  Input : 24 V

  Fixed OutPut : 5V

  Output current : 200mA to 500mA

 Low noise , high accuracy 

 

Now i plan to use ADP7142,  have a better choice?

 

Outcomes