AnsweredAssumed Answered

During debug exception

Question asked by GKRAO on Jul 30, 2018
Latest reply on Aug 10, 2018 by Jithul_Janardhanan

I'm using BF-609 in one of our Hardware.

After Power ON,the JTAG has been connected to the Hardware and passed the jtag configuration test (scan path) but during debug we got the exception (as attached) at the very first at adi_initComponents() and the application has been halted.
I have tried the following options i.e

1.  Cleaned and re-built the project.
2.  Created new project in the new workspace with default settings of BF609 ,built and loaded using ICE-2000 emulator.

I had tried with new project with empty code(just c code with simple for loop) as well as with the available examples provided in the CCES IDE (1.1.0) with our Hardware Card in different workspaces  but the code is generating the same exception at the very first at adi_initComponents().

Please post the solution to this exception.

Outcomes