AnsweredAssumed Answered

LTC4000

Question asked by HOD on Jul 29, 2018
Latest reply on Jul 31, 2018 by MartyM

Hi

 

I am planning to design using the LTC4000
I'm thinking about connecting with the LTC3703, but are there any problems


Regarding DCDC's request
VIN: 5-60 V
VOUT: 45 to 60 (maximum power: 200 W)
* In regard to the system, regardless of step-up / step-down / step-up / step-down

Finally LTC 4000 ...
Output CV mode: 42 V maximum CC mode: up to 4.7 A Up to 200 W as output

 

Best Regards

HOD

Outcomes