AnsweredAssumed Answered

Instruction to boot ADSP-21469 EZ-BoardTM

Question asked by ekrogh on Jan 9, 2012
Latest reply on Jan 10, 2012 by Harshit.Gaharwar

Hi

 

We are using the ADSP-21469 EZ-Board. It is configured to use SPI Slave boot mode, the host side of which I'm debugging now.

 

Question:

Is there an C/C++ and/or Assembler instruction that I can make the ADSP-21469 execute, that brings the cpu into the selected boot mode (SPI Slave for now)? That is: An instruction the ADSP-21469 that results in the same as pressing Reset or power Off-On ?

 

 

Thanks in advance

Eigil

Outcomes