AnsweredAssumed Answered

AD9484-500EBZ connect to HSC-ADC-EVALCZ test

Question asked by 俊采星驰 on Jul 26, 2018
Latest reply on Aug 14, 2018 by David.Buchanan
Hello, I bought AD9484-500EBZ and HSC-ADC-EVALCZ. I want to connect them together for testing. But I didn't test the waveform. Where am I doing wrong? The requirements for analog signal and clock signal can give a detailed explanation, thank you. The impedance of the signal source is highz or 50 Ω .The 1.5 V pp,is there a bias,for example of 0.75V. Can I set the frequency of the clock signal to 100MHz? Is there anything else to pay attention to in the operation of the software?
In addition, I want to make use of the clock source AD9517-4 on the board, how to operate, how to configure the software  to get the frequency of 500MHz, thank you.I'm looking forward to your reply,thank you!

Outcomes