AnsweredAssumed Answered

Unabke to Programming u-boot in ADZS-SC589-EZLITE

Question asked by arun.mishra on Jul 26, 2018
Latest reply on Jul 30, 2018 by arun.mishra

Hi,

I am trying to load u-boot in ADZS-SC589-EZLITE eval board and following the same steps as given in 

Linux_Add-in_User's_Guide-1.2.0.pdf  section 2.1.3, the bmode pin is set to 1 (SPI2 master boot. Default boot mode).

When I run the given command 

/opt/analog/cces/2.6.0/ARM/openocd/bin/openocd -f interface/ice1000.cfg -f target/adspsc58x.cfg

 

I got following prints

Open On-Chip Debugger (Analog Devices CCES 2.8.0 OpenOCD 0.9.0-g5030ad7) 0.9.0
Licensed under GNU GPL v2
Report bugs to <processor.tools.support@analog.com>
adapter speed: 1000 kHz
Info : transports supported by the debug adapter: "jtag", "swd"
Info : auto-select transport "jtag"
halt and restart using CTI
trst_only separate trst_push_pull
Info : ICE-1000 firmware version is 1.0.2
Info : clock speed 1000 kHz
Info : JTAG tap: adspsc58x.adjc tap/device found: 0x228080cb (mfg: 0x065, part: 0x2808, ver: 0x2)
Info : JTAG tap: adspsc58x.dap enabled
Info : adspsc58x.dap: hardware has 3 breakpoints, 2 watchpoints
Info : adspsc58x.dap: but you can only set 1 watchpoint

 

After which the command prompt got stalled.Also the status LED of ICE-100 turned Magenta from green.

Can you suggest what is the problem. Are the steps I am following and bmode setting correct ?

 
 

 

 

Outcomes