AnsweredAssumed Answered

I can't see the entire window of ADRV9009 plugin

Question asked by Sylvain.L on Jul 25, 2018
Latest reply on Aug 7, 2018 by aardelean

Hello,

 

 

I have recently installed the ADRV9009 on my ZCU102 board. 

 

The IIO Oscilloscope starts with the "ADRV9009" and "ADRV9009 Advanced" tabs, but there is no scrollbar on the "ADRV9009 Advanced" tab (see picture bellow).

 

 

This means that I can't have access to the settings bellow the screen, and I can't click on "Save Settings" ....

 

I have tried the different possibilities to see the entire window :

 

- reshape the window : possible on the side but not on the vertical direction, for an unknown reason...

 

- change the resolution / turn the screen with the "xrandr" command : not possible

analog@analog:~$ xrandr
xrandr: Failed to get size of gamma for output default
Screen 0: minimum 1280 x 800, current 1280 x 800, maximum 1280 x 800
default connected 1280x800+0+0 0mm x 0mm
1280x800 0.0*

 

- change the screen : no difference

 

- use Display port / VGA : no difference

 

- zoom / unzoom the screen : not possible

 

Do you have any ideas ?

 

 

Thank you,

Sylvain

Outcomes