AnsweredAssumed Answered

AD9361 ctrl_in pin swap

Question asked by thor@so-logic.net on Jul 24, 2018
Latest reply on Jul 25, 2018 by sripad

We are using the fast lock profiles to switch with the ctrl pins , but it seems that the pins are shifted from the data sheet Ref F

According the data sheet ctrl_in[2:0] should be used, but this didn't not work, we got only 4 frequencies instead of 8 out.

Now we use ctrl_[3:1] and it works fine.

We measure it also on our PCB and it works also if we switch them with the SPI command.

 

Please can you confirm, that this is an bug in data sheet.

Outcomes