AnsweredAssumed Answered

Unable to set breakpoints in CCES with ADSP-SC589 EZ BRD on DSP cores

Question asked by tchadwick@kvh.com on Jul 23, 2018
Latest reply on Jul 27, 2018 by GrahamNewton

If I set a breakpoint in one of the DSP cores, when I try to debug I get the error message "Failed to set breakpoint at C:\Users\tchadwick\cces\2.8.0\testCore1_Core1\src\testCore1_Core1.c [line: 26] because there is no debug line info.".  I checked the settings and it says that it should be generating debug information (-g option to the compiler).  I can set breakpoints in the ARM core but can't in either of the DSP cores.

Outcomes