AnsweredAssumed Answered

HMC960LP4E output characteristics

Question asked by diverger on Jul 21, 2018
Latest reply on Aug 1, 2018 by diverger

The HMC960LP4E's input impedance can be set to differential 100 or 400 Ohms. But how about the output impedance?  In the data sheet, it states:

 

 

  1. The full scale output changes with load, why the span cut a half when the load is 100 Ohms? Does this imply HMC960 is not low output impedance, but has fixed output impedance?
  2. The 'Output Voltage Range' means the each single end output voltage range, right?

Outcomes