AnsweredAssumed Answered

2018_R1-2018_06_26.img on ZC706 and ADRV9371

Question asked by DSPdesigner on Jul 20, 2018
Latest reply on Jul 20, 2018 by DSPdesigner

Hello I have downloaded 2018_R1-2018_06_26.img image from AD website and burnt it onto an SD-card.

I copied BOOT.BIN, devicetree.dtb, and uImage from the relevant sub-directories into the root directory of the BOOT partition of the SD card. 

However, when I am attempting to boot the system I am getting the following printout at the serial console.

Why is the system unanble to read devicetree.dtb?

 

Please advise.

 

 

U-Boot 2014.07-dirty (Nov 20 2014 - 17:07:55)

Board: Xilinx Zynq
I2C: ready
DRAM: ECC disabled 1 GiB
MMC: zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 512 Bytes, erase size 128 KiB, total 32 MiB
In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 0
Device: zynq_sdhci
Manufacturer ID: 74
OEM: 4a60
Name: SDC
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.7 GiB
Bus Width: 4-bit
reading uEnv.txt
407 bytes read in 29 ms (13.7 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
reading uImage
4109416 bytes read in 375 ms (10.5 MiB/s)
reading devicetree.dtb
** Unable to read file devicetree.dtb **
Copying Linux from SD to RAM...
reading uImage
4109416 bytes read in 374 ms (10.5 MiB/s)
reading devicetree.dtb
** Unable to read file devicetree.dtb **

Outcomes