AnsweredAssumed Answered

GUIs for ADRV9009

Question asked by Sylvain.L on Jul 20, 2018
Latest reply on Jul 24, 2018 by Sylvain.L

Hello,

 

 

I'm trying to use the ADRV9009 on a ZCU102 board but I have two problems :

 

1. On the linux of the board

 

It boots, I can see the IIO Oscilloscope, and the ADRV9009 is detected but I can't find how to get the ADRV9009 plugin for the IIO Oscilloscope described here : https://wiki.analog.com/resources/tools-software/linux-software/adrv9009_plugin 

 

How do I find it and install it on the linux of the board ?

 

 

2. On my PC connected to the ZCU102

 

I have a PC connected to the ZCU102, running the ADRV9009 GUI. The problem is that it doesn't detect the ADRV9009.

I am connected with a UART and ethernet links to the board.

 

I have checked the IP adresses:

- The TCP IP of the ZCU102 is 127.0.0.1 and I've tried the ports corresponding to this adress on my PC, they don't work, I get the message "Cannot Connect to the Device. Please Check IP Adress And/Or Port Number". 

 

- However, the UDP adress of the board is the same as detected of my PC, on the port 546, but I can't give a UDP adress to the ADRV9009 GUI.

 

 

Also, I don't really get the difference between the ADRV9009 GUI and the ADRV9009 plugin of the IIO Oscilloscope.

 

 

Thanks,

 

Sylvain

Outcomes