AnsweredAssumed Answered

AD8032,8031 Rev

Question asked by HOD on Jul 19, 2018
Latest reply on Jul 25, 2018 by HOD

Hi

 

I have a question AD8032,8031 Rev.

I would like to check about the correction points of the data sheet

 

REV.

変更内容

  

3/14Rev. F to Rev. G

Changes to Second Paragraph of Theory of Operation Section ... 13

It will look like no change. What has changed?

  

Changes to Ordering Guide ......................................................... 20

Although it seems that the annotation notation of the text is gone, it seems that "1" stating "1 Z = RoHS Compliant Part, # __ lead - free product may be top or bottom marked." Remained

8/13Rev. E to Rev. F

Changed Input Current Noise at f = 100 kHz from 2.4 pA/Hz to 0.4 pA/Hz (Throughout) .......................................................... 3

(DISTORTION / NOISE PERFORMANCE) Input Current Noise (f = 100 kHz) (Before change) 2.4 (after change) 0.4 Positive change?

6/13Rev. D to Rev. E

Changes to DC Performance Parameter, Table 1 ......................... 3

It seems unchanged

 

Best Regards

HOD

Outcomes