AnsweredAssumed Answered

Can't connect IIO oscilloscope application with VC707: FMCDAQ2 example build

Question asked by AMIT_SANGWAN on Jul 19, 2018
Latest reply on Aug 10, 2018 by aardelean

I am facing connection issue and trying to debug it.

When I launch the IIO application (windows 7) it shows that no iio device found.

In the boot log it says that the device AD9680 and AD9144 are properly connected and IIO daemon server started.

 

Please find the attached log of the start.
I am using a VC707 board and DAQ2. I used the pre-built image of the .bit and the image file

as mentioned in the tutorial wiki:

link to page: AD-FMCDAQ2-EBZ/AD-FMCDAQ3-EBZ on Microblaze [Analog Devices Wiki]  

Link to download: http://swdownloads.analog.com/cse/microblaze/2018_r1/2018_r1_vc707_fmcdaq2.zip (FMCDAQ2 2018_R1 version of files)

 

Kernel_Boot_log

Outcomes