AnsweredAssumed Answered

Is address command available on LTC6811-2 4-wire SPI ? Can we parallel 2 or more LTC6811-2 using the same CS  and the address selection ?

Question asked by mohamed.jaidane@visuray.com on Jul 19, 2018
Latest reply on Jul 30, 2018 by vchandra

Is address command available on LTC6811-2 4-wire SPI ? Can we parallel 2 or more LTC6811-2 using the same CS  and the address selection ?

I would like to use a modular system for monitoring battery cells with an unknown number of modules to be connected. So the addressing scheme seems perfect but I cannot confirm if this is available for the SPI 4-wire on the LTC6811-2 or it's only for IsoSPI.

Outcomes