AnsweredAssumed Answered

ADA4817-1/2

Question asked by PREMSAGAR on Jul 18, 2018
Latest reply on Jul 20, 2018 by PREMSAGAR

Hello, 

I am looking for a buffer (Analog) with the following requirements: 

1) Input voltage range: 0V to 0.9V 

2) Fq: ~100MHz to 200MHz 

3) Iq, Noise: We don't really care about it 

4) VDD: We can provide any VDD between 0.9V to 3.3V (Or may be even higher if needed)

5) Should have very (very) low input capacitance. Kind of main requirement for this buffer. (May be less than 1pF?? I know its difficult to get it) If input doesn't have ESD protection, it will work for us.

6) Input is single ended 

 

I searched the website and found ADA4817-1/2. Is this the closest product for our specs or do you suggest some thing else?

 

Thank you!

Outcomes