AnsweredAssumed Answered

AD9956 big doubt

Question asked by rodney on Jan 5, 2012
Latest reply on Jan 6, 2012 by Kevin.G

Hello,

 

I´m designing a circuit based on ADI´s AD9956 like the typical aplication circuit showed on Figure 24. LO and Baseband Modulation Generation" AD9956 datasheet, page 16.

 

typical.JPG

On page 12 says:

 

PIN   Mnemonic         Description

20     I/O_UPDATE     This input pin, when set high, transfers the data from the I/O buffers  to the internal registers on the rising edge of the internal                                  SYNC_CLK,  which can be observed on SYNC_OUT.

 

On that typical application the SYNC_CLK signal is the output of R divider, and the PLLref signal is provided by a crystal. But, i need that AD9956 recognice the I/O_Update signal to:

- Enable cristal oscillator

- Configure CML driver

- Configure R diveder

-Configure N and M dividers.

- Others configuratons.

 

How is it possible if I dont have the SYNC_CLK signal when I start AD9956?

 

For example, on AD9912 from ADI too the I/O_Update signal is completely asynchronous.

 

Can some one clear my doubt?

Outcomes