AnsweredAssumed Answered

LTM8055

Question asked by ramidamari on Jul 18, 2018
Latest reply on Jul 18, 2018 by Jeoffrey

Hi

I am using this umodule, in order to get 24V 6A from 18V-36V. I noticed that when the current is more than 3A, VOUT starts to derate to 14V and less. I a dont limit current in or out.

I also noticed that efficiency is ~60%.

 

When I checked the EV I saw the same problem

 

It is odd that there is no graph  on the datasheet regarding VOUT vs Current out

 

Does anyone have the same problem?

 

Rami Damari

Outcomes