AnsweredAssumed Answered

Connecting 2 FMCOMMS5 board with a single Zc706 carrier board !

Question asked by tancarrerece on Jul 18, 2018
Latest reply on Jul 18, 2018 by tancarrerece

Hello,

I'm working on FMCOMMS5 board with the xilinx ZC706 SoC as carrier board. At a time one such FMCOMMS5 can be attached with the zc706 board through 400 pin HPC FMC interface.  I have 2 units of FMCOMMS5 boards and I was thinking of using both of them connecting them simultaneously through the HPC interface with the help of some 1 to 2 cabling arrangement. Is this possible? If so, where I can find such a connector? 

Thanks,

Tanmoy

Outcomes