AnsweredAssumed Answered

ADXL355

Question asked by HOD on Jul 18, 2018

Hi

 

I have a question ADXL355.

 

Data sheet p22
Please tell me about over range protection specification of ADXL 355.

"Floating state towards zero", but in the case of the axis in the direction of gravitational acceleration,
Can I think that it costs 1 G offset?
When applying sinusoidal vibration of 1 G or more in the direction of gravitational acceleration, the value of the sinusoidal vibration around 0 G was output.

Below is the setting environment.
· Input vibration: 20 Hz amplitude 1 G stronger
· Sensor setting: Range ± 2 G ODR 250 Hz External sample mode (measurement frequency 200 Hz)

 

Best Regards

HOD

 

 

Outcomes