AnsweredAssumed Answered

Is ADE9000 suitable for 400Hz avionic grid applications?

Question asked by ferario on Jul 16, 2018
Latest reply on Jul 17, 2018 by Gary.Kang.AnalogDevices

ADE9000 has two set of measurements:

 

-         Total active energy, total reactive energy, total apparent energy, IRMS, VRMS  can be calculated  for 400Hz applications as well, since the AFE band is 3.2K

-        My concerns are about fundamental active/reactive/apparent/current rms/voltage rms measurements since the PLL that extract the fundamental frequency has been tuned on 45Hz to 65Hz range.

-     Is there any AFE capable of 400Hz fundamental active/reactive/apparent measurements?

Outcomes