AnsweredAssumed Answered

adau144x TDM8 on scope

Question asked by benybiles on Jul 14, 2018
Latest reply on Jul 30, 2018 by DaveThib

Hi , I am new to working with TDM8 24bits

 

I have adau144x working in master mode

 

The DSP is working in pulse mode in TDM8 24bit mode.

 

I have delayed by one set ( i2s mode )

 

So I calculate there should be 32 fs clocks per slot x 8 slots = 256 fs clocks for the whole frame between pulses.

 

It appears that I have maximum of 20bits of audio in the middle of the slots with 8 bits either side.

Also I have on the left what seams like strobing bits accross the 1st 24bits ( left to right )  with nothing in the last 8bits (right )

 

the sclk is 12.288mhz

FS is 48khz

 

The ADAU1446 is master on TDM8 bus. 

 

here's some pics from the scope.

TDM8

the single slot,

 

My question really is , does anyone have a clue what could be causing the strobing across the 1st 24bits?

or is this normal for TDM8 ?

 

 

[EDIT]

 

I wasn't seeing the 1st 8 - 10 bits since I never got anything load enough out of the DSP. I set tone to 100% and the full dynamic range of the 24bits is used.

 

So that only the question about the line across the top of the bits on the scope. Is this expected ?

 

I tried unconnected my ARM proto board as its quite noisy and I still get the top line from the DSP.

Outcomes