AnsweredAssumed Answered

ADS7-v2 EVM FMC connector supply issue?

Question asked by aliBugra on Jul 13, 2018

Hi, I have a ADS7-v2 EVM and AD9208 EVM boards. Up to now, I have used ACE application to implement ADC data capturing. However, from this point, I want to create my own embedded design into FPGA. When starting, I recognized that 1.8V, 3.3V and 12V supplies of FMC connector on ADS7-v2 is controlled and can be opened by Blackfin DSP processor. Is it possible to open FMC connector voltage without embedding programme into DSP processor on ADS7-v2? It would be great for me if I can realize ADC data capturing procedure by implementing only FPGA code. Or do you have a basic DSP processor code for open these voltages?

Outcomes