AnsweredAssumed Answered

AD-FMCOMMS4-EBZ and its HDL reduce resources

Question asked by proxcmos on Jul 12, 2018
Latest reply on Jul 18, 2018 by AdrianC

Hi ,,

 

I'm using ad9364 and ZedBoard

 

since the hdl labelled "fmcomms2" can be used for all different fmcomms2/3/4 boards .. I want to modify the hdl to use only one Rx/Tx  for ad9364 .. fmcomms2 has 4 channels (i0,q0,i1,q1) ...

 

 

what things I should change?

 

for example, Do I need to change MODE_1R1T in AXI_AD9361 component.

configure upack and cpack utility to delete the second channel! 

 

what about clocking! is it going to give me more data rate instead of 61.44! or it is limited by the chip and interface type (cmos - lvds) as I understand!

 

The reason I'm doing that is to reduce fpga resources!

 

thanks 

Outcomes