AnsweredAssumed Answered

AD7177-2在±2.5V供电下的模拟输入电压范围

Question asked by gl1995 on Jul 12, 2018

我最近在看AD7177-2这款32位ADC,我打算是用±2.5V给它供电。但是我看到技术手册中的 额定最大电压里写到:analog input voltage to AVSS:-0.3V to AVDD1+0.3V ,当我用分离电源时,AVDD1=2.5V,AVSS=-2.5V,那么根据手册中说的,每个模拟输入端的电压不就只能是在-2.8V到0.3V之间? 本来以为单端模拟输入电压能在±2.5V之间摆动的,感觉很困惑。

 

求大神给我解答!!!

Outcomes