AnsweredAssumed Answered

Unable to read File Image Error

Question asked by siddh4nt on Jul 12, 2018
Latest reply on Jul 16, 2018 by DragosB

Hi everyone,

 

I followed the instructions given here : Windows Download and setting up the image [Analog Devices Wiki] , also I copied the required files to base folder, I tried to boot my board and got following error:

 

In: serial@ff000000
Out: serial@ff000000
Err: serial@ff000000
Bootmode: LVL_SHFT_SD_MODE1
Net: ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

Warning: ethernet@ff0e0000 using MAC address from ROM
eth0: ethernet@ff0e0000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 3
OEM: 5344
Name: SD08G
Tran Speed: 25000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.4 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uEnv.txt
381 bytes read in 11 ms (33.2 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
Running uenvcmd ...
Copying Linux from SD to RAM...
** No boot file defined **
reading system.dtb
43396 bytes read in 67 ms (631.8 KiB/s)
reading Image
** Unable to read file Image **
ZynqMP>

 

 

Any Suggestion?

 

 

 

Thank you

-Siddhant

Outcomes