AnsweredAssumed Answered

AD9371 Tx and Rx profile gen through Filter Wizard

Question asked by boyapati_hari on Jul 11, 2018

In simplest configuration, i would like to configure AD9371 for following tx and rx configurations through filter wizard.

we are more familiar to AD9361 settings.

Tx settings:

TX sampling frequency: 5 MHz

TX bandwidth : 5  MHz

In this case data clock is 10 MHz.

Rx settings:

RX  bandwidth is 10 MHz and sample rate is same as 10 MHz and Data Clock is 20 MHz in SDR mode of configuration (Single Data Rate, Full Duplex)

 

Please help me in generating custom configuration in similar lines as AD9361.

 

In filter wizard i have tried to put the settings but it is throwing error.

 

Note: Can i get material to understand the AD9371 filter wizard.

Outcomes