AnsweredAssumed Answered

How to Monitor Backlash in Gear

Question asked by momin.naseh3@gmail.com on Jul 11, 2018
Latest reply on Jul 11, 2018 by NevadaMark

Dear Sir/Madam,

             I am Working on R&D Project entitled " Monitoring Lateral Misalignment and Backlash in Spur Gear using Proximity Sensor". I had completed my research work up to Monitoring Misalignment using analog Proximity Sensor but I am unable to find Backlash (Reducing one gear teeth thickness by 1 mm).  Please suggest me a suitable sensor so that I can conclude my research.

1) Gear Box is having single gear pair only.

2) DC Motor having Max 1500 RPM

3) OD of Gear is 150mm

4) Diametral Pitch is 8

5) Number of teeth is 45.

 

 

 

Thanks and Regards

Naseh Momin

FCRIT Vashi 400073

Indi

Outcomes