AnsweredAssumed Answered

EXTCLK application for AD7768-1

Question asked by @Linear on Jul 10, 2018
Latest reply on Jul 10, 2018 by @Linear

Due to some special demands, we need to use External XTAL.

But we can not find the input voltage of EXTCLK. Could you help to check this issue on AD7768?

 

Now our XTAL is 10MHz@0.8V, sinewave, low jitter and drift. We can not make sure it can work on AD7768-1 or not.

Please also help to check the min voltage input for EXTCLK, and remind to double check in the datasheet if necessary.

Thank you very much.

 

B.Regard,

Linear

Outcomes