AnsweredAssumed Answered

Analyzing the ADSP 21469 anomalies

Question asked by Rpentyala on Jul 9, 2018
Latest reply on Jul 17, 2018 by Jithul_Janardhanan

Hello,

 

I am trying to understand the anomaly provided by AD on ADSP-21469 and during the course came across couple of questions/clarifications.

 

Visual DSP ++ 5.0 Update 8 used to compile and load program into target. ADSP-21469 Silicon Revision 0.2 used in program and while going through the anomalies many were mentioned about ( please consult the "Silicon Anomaly Tools Support" help page in the applicable documentation and release notes for details.). Not sure what that means...

 

For example refer to adsp-21467_21469-sharc-anomaly.pdf 

15000002 anomaly workaround section.

 

Having tough time to understand some of the anomalies listed in the document. 

 

Our project configuration is as follows:

All of the processor specific library functions configured in 48-bit space and in internal memory.

Application code configured as 16-bit VISA and stored in internal momery

Complete data memory configured in external DDRAM as 32-bit.

 

with the above information, is there a way to figure out which anomalies applicable and which are not?

 

Any comments or feedback on this highly helpful

 

Thanks

Ram

Outcomes