AnsweredAssumed Answered

AD9788-DPG2-EBZ: how to set registers

Question asked by giusloq on Jul 6, 2018
Latest reply on Jul 19, 2018 by deljones

I have the evaluation board specified in the title. I can use "AD9788 SPI" and "AD9516 SPI" applications to control the two ICs AD9788 (TxDAC) and AD9516 (clock generator) mounted on the board.

 

However I couldn't understand if these GUI applications let me set freely the registers over SPI. For example, I'd like to use the internal SRAM of AD9788, instead of using real input signals on I and Q ports. In order to enable the data RAM, I need to write the value 0x00C000 into the Test register (0x1E). Is it possible with "AD9788 SPI" application?

Outcomes