AnsweredAssumed Answered

BIST tone test ad9361 using TxMonitor (RSSI)

Question asked by tancarrerece on Jul 6, 2018
Latest reply on Jul 9, 2018 by DragosB

Dear engineers and researchers,

 

I'm using FMCOMMS5 and Xilinx zc706, No-OS API. I want to generate a BIST test signal using ad9361_bist_tone(ad9361_phy, BIST_INJ_TX,3,0,0) and directly couple that tone to TXMON_1(or2) port using an RF cable connector. so that I can measure the incoming signal power level. I have some questions:

1. Is it safe to connect TX and TMON port directly using a cable?

2. If not then what I have to do if I want to measure the power level in that fashion? 

3. In this case is it useful to use the ad9361_set_tx_attenuation function, or I can manually control the gain at the RX during the RSSI measurement? 

 

Thank you,

Tanmoy

Outcomes