AnsweredAssumed Answered

0.9V VOUT LDO REQUIRED

Question asked by PREMSAGAR on Jul 4, 2018
Latest reply on Jul 13, 2018 by PREMSAGAR

Hello,

 

I am looking for an LDO with Min Vout = 0.8V to Max Vout = 1.2V. Vin is adjustable (always greater than 2V). Iload expected is about 100mA at Vout = 0.8V. It is for an application running at ~100MHz, so PSRR should be around 20-25dB at this frequency (not a strict requirement). We don't really care about the power consumption of the LDO, capped or capless LDO.

 

So is LTC3035 the best match for our specs..??

Outcomes