AnsweredAssumed Answered

AD5560_Shutdown

Question asked by superbeginner on Jun 28, 2018
Latest reply on Jul 1, 2018 by superbeginner

hello

 

I am using the AD5560 to measure the temperature by making a current of 500 mA.

 

1: There is a channel which shuts down when measuring 500 mA at 1 Ω resistance and 0.5 V applied voltage.
2: not shut down when measuring 500 mA with resistance 10 Ω, applied voltage 5 V.

 

1 Ω, the measurement temperature in TSENSE immediately after application is around 75 ° C
When it is 10 Ω, the measurement temperature at TESENSE immediately after application is around 58 ° C

 

AD5560, depending on the resistance value to be used, is there a short circuit condition, upper limit value, lower limit value etc?

 

Could you tell me

Outcomes