AnsweredAssumed Answered

AD7865 supply voltage

Question asked by ianstedman on Jun 28, 2018
Latest reply on Jul 4, 2018 by ianstedman

Hi,

The AD7865 is specified to operate from an AVDD supply of 5V +/-5%. What would happen to the sampled data if it is operated outside of these 5% limits?

In a legacy design, the AVDD pins is connected via a simple RC low pass filter, R is 10 ohms and C is 100nF. A DC measurement was 4.76V at ambient, indicating 24mA of current. At datasheet maximum current of 32mA, Avdd would be 4.68V. We use an external Vref (2.6V)  for the device and DVDD and Vdrive are connected to +5V directly.

I'm seeing some odd results in the analogue signal chain and need to rule out options.

Outcomes