AnsweredAssumed Answered

HMC703LP4E reference input slew rate

Question asked by sss on Jun 26, 2018
Latest reply on Jul 13, 2018 by dyoung1

Hi all,


In the datasheet about reference input,
Slew rate of greater or equal to 0.5 V/ns, it is recommended at low frequencies, a relatively square reference is recommended to keep the input slew rate high.

 

Is it only rising, falling, or both edges ?

In general,, Falling edge degradates the slew rate.

 

I think the phase detecter block is trigered rising edge from ref/R and RF/N.
Is it correct ?
Is it difference from ADI PLL and Hittite PLL about edge detect ?

Dose the slew rate of falling edge affects the phase detecter function?

 

Best regards,

sss

Outcomes