AnsweredAssumed Answered

ADV7181C配置需求

Question asked by hackathos on Jun 25, 2018
Latest reply on Jul 16, 2018 by Poornima

 目前我们有一个项目使用了ADV7181C,已焊机回板,目前正在测试,使用方式如下:

1、使用红框中的数据输出格式;

2、输出分辨率:1280*720

 Adv7181的输入是vga rgb信号,分辨率时720p;我们需要adv7181转化后的输出是12bit 4:4:4 rgb ddr

现在的问题是:

adv7181输入单色的r信号,输出的是r

adv7181输入单色的b信号,输出的是b

adv7181输入单色的g信息,输出还是r

 

adv7181丢了一种颜色,不知道为什么?

我使用的配置如下:

i2c_write 0 0x42 0x5  0x1

i2c_write 0 0x42 0x6  0xa

i2c_write 0 0x42 0xc3 0x56

i2c_write 0 0x42 0xc4 0xb4  

i2c_write 0 0x42 0x1d 0x47  

i2c_write 0 0x42 0x3a 0x21

i2c_write 0 0x42 0x3b 0x61

i2c_write 0 0x42 0x3c 0x5d

i2c_write 0 0x42 0x6a 0x0

i2c_write 0 0x42 0x6b 0x84  

i2c_write 0 0x42 0xc9 0x8

i2c_write 0 0x42 0x73 0x90

i2c_write 0 0x42 0x7b 0x1d  

i2c_write 0 0x42 0x85 0x3

i2c_write 0 0x42 0x86 0xb

i2c_write 0 0x42 0xf4 0x3f

i2c_write 0 0x42 0x0e 0x80

i2c_write 0 0x42 0x52 0x46

i2c_write 0 0x42 0x54 0x00

i2c_write 0 0x42 0xf6 0x3b

i2c_write 0 0x42 0x0e 0x00

i2c_write 0 0x42 0x52 0x80

i2c_write 0 0x42 0x57 0x08

i2c_write 0 0x42 0x5b 0x20

i2c_write 0 0x42 0x5c 0x00

i2c_write 0 0x42 0x62 0x00

 另外我们这中输入(vga rgb 720p)输出(12bit 4:4:4 rgb ddr)方式,你们有推荐的配置吗?

Outcomes