AnsweredAssumed Answered

About LED flash driver ADP1660

Question asked by Mars.Chang on Jun 25, 2018
Latest reply on Jul 11, 2018 by JonD

Dear all,

 

My customer has two laser diodes ( 450mA per ch)

About the ADP1660 LED flash driver function, I see the spe has several mode,


e.g.

LED_MOD Bits

101
Independent trigger mode with timeout disabled (FL_TIM value is ignored)
110
Fixed 5 V output mode with torch mode (total output current must be below 500 mA)

 

 


If I want to do below behavior, which mode can do this?

Outcomes