AnsweredAssumed Answered

SOM2 usage for end application

Question asked by Kalkikrishna on Jun 22, 2018
Latest reply on Jun 25, 2018 by Kalkikrishna

We want to use SOM2( ADRV9361-Z7035) for our end application system which may need to undergo environmental qualifications. Since in the same board two RX and two TX chains are routed, whether it can pass the EMI/EMC qualifications provided we do proper shielding of the module with aluminium enclosure. Our temperature specs are -40 to +85 deg C. Since the micro SD card cage on the SOM doesnt meet this temperature spec whether we can remove the micro SD card.We may use either as TXR or RXR . Please clarify

Outcomes