AnsweredAssumed Answered

AGC customization for AD9364 with No-os drivers

Question asked by prasadgedelarb@bel.co.in on Jun 22, 2018
Latest reply on Jun 25, 2018 by sripad

Hi all,

  We designed a AD9364 based board and could successfully test it in Manual gain control mode i.e., rx_gc_mode = 0. The following are the design parameters.

center frequency = 4 GHz

Bandwidth = 26 MHz

sampling rate = 30.72 MHz

Mode of Operation = FDD

Frame size = 5 ms

Though it is a continuous link, we perform receiver tuning and channel estimations only on the preamble portion i.e. at the start of every 5 ms. Change in gain value within the 5 ms (after preamble) period  lead to a scaling (x2, x0.5 etc) which is different from the scaling seen at preamble. This results in wrong decoding, since the demodulation threshold are fixed w.r.t the modulation (QAM ).

When slow attack agc mode is enabled, less frequent symbol errors are observed even with a constant power at the receiver input. But in fast attack mode errors are very frequent. Please suggest us the appropriate mode and corresponding parameters for the described case.

 

Thank in advance,

 

raj@@

Outcomes