AnsweredAssumed Answered

The signal transmission about the AD9371

Question asked by feixiang on Jun 20, 2018
Latest reply on Jun 27, 2018 by sripad

    I set the TX/RX LO  750MHz, and the TX IQrate 307.2MSPS, and the RX IQrate 153.6MSPS, when I transe the 5MHz signal ,the RX signal is perfect, but when I transe the 30MHz signal ,the RX signal is distortion .

 

the parameters I configure the AD9371.

the transaction parameters.

there is the signal envelope  in the RX signal.

When  I transe the5MHz, the RX signal is perfect.

Outcomes