AnsweredAssumed Answered

Problem with external VREF AD9629

Question asked by crazyfrog on Jun 18, 2018
Latest reply on Jun 19, 2018 by DougI

Hi all,

 

I have design a board using an ADC AD9629, combined with a differential amplifier ADA4940.
It works fine in normal mode. In normal mode I m measuring single pulses from 0V to 6V to VIN without any issue at 10Msps.
I have used an external reference ADR130BUJZ, in order to compensate the temperature variation of my system.

 

I have an additionnal DAC (MAX5815) which goes to VIN.  This DAC apply a DC signal to VIN. With this DAC, I can create a lookup table (in my software) to compensate the gain error.

 

However, am seeing something odd: Whenever i change the DAC value with the ADC clock ON, my external VREF goes from 1V to 0V. Then the Adc is blocked, I have got to unplug my board.

 

What can create this issue?

Attachments

Outcomes