AnsweredAssumed Answered

Do I must use the PIN MASTER_RESET in AD9911?

Question asked by IHPGY on Dec 25, 2011
Latest reply on Jan 18, 2012 by Kevin.G

Hello, I am working on the AD9911 with a DSP. In the control line, I found this device do not have a pin I/O_RESET as in AD9910, and I confused with use of reseting device.

 

Does this pin MASTER_RESET must be  connect out and be used?  When starting up AD9911, do I must reset AD9911?  In my current design, I made this pin fixed connected with GND and do not connected to DSP. Untill now this DDS device works well but I am worried when no signal comes out how could I reset it and make it right. Thank you very much.

Outcomes