AnsweredAssumed Answered

AD8015: temperature stability of pin Vbyp

Question asked by Alena_K on Jun 17, 2018
Latest reply on Jun 19, 2018 by ARoxas

Hello, I have some questions about AD8015:

1. What is maximum output current for pin Vbyp?

2. I need to stabilize voltage on pin Vbyp to work in wide temperature range (from -20C to +70C). For positive supply we have +2.1V and for negative supply -5V. So, I just connected pin Vbyp through 51 Ohms resistor to ground. This allowed to reduce the drift voltage at the pin Iin from 150 mV to 10 mV. Is it correct? Are there any other ways to stabilize voltage on pin Vbyp?

Outcomes