AnsweredAssumed Answered

ADC Eval board and Data capture board

Question asked by Radarrr on Jun 16, 2018
Latest reply on Jun 17, 2018 by UmeshJ

Hello. I am going to use the ADC evaluation board and data capture board as a baseband receiver for radar. Since BW of about 500MHz ~ 1GHz is used, Sampling rate of 2GHz or more is sufficient. The ADC products I am thinking of are the AD9625, AD9208, and AD9689. The corresponding data capture boards are HSC-ADC-EVALCZ and ADS7-V2EBZ.
I'm curious
1. Using the ADC evaluation board and the appropriate data capture board, is it okay to receive data from a computer like a typical Oscilloscope?
2. It seems to collect data using visual analog. I would like to process the radar signal in real time while collecting data. Is it possible?
3. Can I collect data using Matlab or other methods without using Visual analog?

I am always getting a lot of help. Thank.

Outcomes