AnsweredAssumed Answered

DUAL PORT FDD FUNCTIONAL TIMING (CMOS)

Question asked by stefanardo on Jun 14, 2018
Latest reply on Jun 15, 2018 by stefanardo

Hi, I need to use AD9361 in DUAL PORT FDD mode with NO-OS software and I do not understand the relationship between the graphs in page 104 of UG-570 and the device driver software.

1)Which function sets the 2R2T mode? Two_rx_two_tx_mode_enable ? with 0 = 1R1T and 1 = 2R2T?

2)Why in the graphs is written 2R2T mode bit in graphs there are only R1_I R1_Q, T1_I and T1Q?

3)I cannot find this UG-570 on analog devices website. Why? Is there an updated version?

4)Are the graph in page 104 correct?

 

Thanks and best regards.

 

 

Stefano

Outcomes