AnsweredAssumed Answered

Is it possible to fine tuning the pitch / volume of the ADAU1401a?

Question asked by Andrew.Choi on Jun 13, 2018
Latest reply on Jun 15, 2018 by DaveThib

Hi AID's

 

One of the customers is developing the ADAU1401a and she wants to control pitch and volume precisely.

she would like to be able to adjust to two decimal places as much as possible to implement the function.

(Assuming that the input signal is 100% frequency, wants to control it like this: 100% -> 102.55%)

In Sigma Studio, the Pitch Shifting and volume controls appear to work only with numbers

I do not think it's supported by blocks, is there any special way?

 

Thank you

Outcomes