AnsweredAssumed Answered

Does the Y/C output of ADV7393 be connected as differential o/p?

Question asked by rajneesh.j on Jun 14, 2018
Latest reply on Jun 15, 2018 by PoornimaSubramani

Hi All,

Greetings!!

I am using the video encoder IC ADV7393 to encode 16bit RGB to Y/C output. But as per the requirement, the output should be differential Y_p/n and C_p/n output. Can the single ended outputs be connected directly to differential output pins of external connector or a single ended to differential converter is required? Or can you suggest a different part that meets the requirement (Analog, 1VP-P terminated condition, differential, 75Ohm).


A block diagram is attached along with.

Thanks and regards,

Rajneesh J

Attachments

Outcomes